Tìm các câu hỏi thường gặp
failed step when applying CU2 on Power Monitoring Expert 9.0 - Execute Installation Scripts
Issue
While installing CU2 on PME 9.0 the installer fails at Execute Installation Script.
![](https://ckm-content.se.com/ckmContent/servlet/servlet.ImageServer?id=0151H000008zrH1QAI&oid=00DA0000000abSm)
Product Line
Power Monitoring Expert 9.0
Environment
PME 9.0 CU2 installer
Cause
The CU installer fails at step Execute Installation Scripts. The install log shows a list of scripts that were not successfully executed.
In this scenario, the installer is not able to run the scripts due to insufficient permissions.
Resolution
A sysadmin account is needed in order to run CU installers.
While installing CU2 on PME 9.0 the installer fails at Execute Installation Script.
Product Line
Power Monitoring Expert 9.0
Environment
PME 9.0 CU2 installer
Cause
The CU installer fails at step Execute Installation Scripts. The install log shows a list of scripts that were not successfully executed.
In this scenario, the installer is not able to run the scripts due to insufficient permissions.
Resolution
A sysadmin account is needed in order to run CU installers.
Đã phát hành cho:Schneider Electric Việt Nam
Tìm hiểu thêm
Phạm vi:
Tìm hiểu thêm
Phạm vi: