How to see a HMISCU Target via USB cable in Vitual Machine
  1. Issue
In a virtual machine, user is able to see PLC M241 but not HMISCU via USB cable in SoMachine V4.3, how to fix the issue?
  1. Environment
VMware and SoMachine V4.3.
  1. Resolution
Normally it is caused by the USB compatibility setting in Virtual Machine, user can change the setting from USB 3.0 to USB 2.0, then the HMISCU Target can be detected in SoMachine V4.3.

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: