Modicon M262 - Programming example with 2 Axis LXM32S - Basic "MoveAbsolute" Sequence

In the attached project, the Motion Controller TM262Mxxxx controls 2 Lexium32S devices over SERCOS III.

Image1

The example program contents a basic:
- Axis configuration 2 Linear Axis without software limits
- Switching ON the power stage (MC_Power)
- Homing the axis (MC_Home)
- Move absolute 2 axis (MC_MoveAbsolute)

Minimum required LXM32S firmware versions:
- LXM32S drive firmware PR912.20 Version >= 1.06.03
- LXM32S SERCOS module firmware PR940.00 Version >= 1.08.04

Schneider Electric Việt Nam

Phần đính kèm

M262_OMK_MoveAbsolute_Example.zipM262_OMK_MoveAbsolute_Example.zip [226.83 KB]
M262_MoveAbsoluteExample.pdfM262_MoveAbsoluteExample.pdf [800.12 KB]
Tìm hiểu thêm
Phạm vi:
Tìm hiểu thêm
Phạm vi: