PME 9.0 - Alarms Library translation in Czech are wrong
Issue
There translation for Recent Events and Recent Incidents are both as "Posledni události" in Alarm tab > "System View"

Product Line
Power Monitoring Expert 9.0

Envoriment
Web Applicatoon - Alarms tab

Cause
The translation for Recent Incidents is wrong in the database, it should be " Poslední Incidenty ".

Resolution
To modify the end text to properly match what the recent events and recent incidents should be in Czech, execute the following query in ApplicationModules database.

EXEC [Internationalization].[WriteLocalizedString] 'cs', 'AlarmClassifications', '', 'ACLS_SystemView_RecentEvents', '', N'Poslední Události'

EXEC [Internationalization].[WriteLocalizedString] 'cs', 'AlarmClassifications', '', 'ACLS_SystemView_RecentIncidents', '', N'Poslední Incidenty'






Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: