Where to find the register list for the Easergy P3 relays?

Issue
Where to find the register list for the Easergy P3 relays?

Product Line
Easergy P3 Standard (P3U10, P3U20, P3U30)
Easergy P3 Advanced (P3F30, P3L30, P3M30, P3M32, P3G30, P3G32, P3T32)

Environment
Document

Cause
Need to know what the registers are for the Easergy P3 relay.

Resolution
The only way to see any register and data type map is to use Easergy eSetup Pro in offline or onlinemode. Once you create an Easergy P3 offline configuration file using “eSetup Easergy Pro software” selecting the modbus protocol, then in the communication section you will automatically see the modbus parameters with the register address.

eSetup Easergy Pro: https://www.se.com/ww/en/download/document/eSetup_Easergy_PRO/

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Tìm hiểu thêm
Phạm vi: