How to find an ION module's handle in ION Setup
Issue
A way to find the handle number for a module in ION template using ION Setup

Product Line
ION Meter
ION Module

Environment
ION Setup

Cause
Be able to find the handle assigned to any ION module

Resolution
1. Using ION Setup, open the device in Advanced Mode
2. Open any module
3. Hold down Control key and click on either Setup Registers or Output Registers tab

The handle number should be shown for each setup or output register.  Here is an example for an External Boolean Module:

Output Registers

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: