PowerChute Network Shutdown 4.3 fails to power off VMware ESXi 6.7 U3 host
Issue:
PowerChute Network Shutdown 4.3 fails to power off VMware ESXi 6.7 U3 host with error

ERROR Thread-82 com.apcc.m11.components.Shutdowner.Hosts.ESXUnmanagedStandaloneHost com.vmware.vim25.RestrictedVersion: Current license or ESXi version prohibits execution of the requested operation.
at java.base/jdk.internal.reflect.NativeConstructorAccessorImpl.newInstance0(Native Method) - hostShutdown

Product Line:
PowerChute Network Shutdown v4.3

Environment:
VMware ESXi 6.7 U3 host with VMware vSphere 6 Essentials Plus license.

Cause:
Change to VMware ESXi 6.7 License

Solution:
User must contact VMware for assistance with the licensing.
Per VMware knowledge base document 1023990 vSphere Essential Plus license should allow CLI access to the host.



Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: