SQL Scripts to Retrieve Security Information from SQL Server
Issue
How to find Retrieve Security Information from SQL Server

Product Line
Struxureware Power Monitoring 7.0.x
Power Monitoring Expert 7.2.x, 8.x, 9.x, 2020
ION Enterprise 6.0. x
ION EEM

Environment
SQL Server 2005, SQL Server 2008 R 2, SQL Server 2012, SQL Server 2014, SQL Server 2016, SQL Server 2017

Cause
SQL Server needs to be configured with an account with the correct permissions.

Resolution
*Warning: Irreparable database damage can occur. This procedure should only be performed by users familiar with SQL Server Management Studio. Databases should be backed up prior to performing this procedure.*

To retrieve the security information of current SQL Server installation, log into SQL Server Management Studio and run the attached SQL script (SQL_Security_Scripts.sql).
Alternatively, execute the query(s) below :

Script to find server level logins and role assigned:

SELECT a.name as LoginName,a.type_desc AS LoginType, a.default_database_name AS DefaultDBName,
CASE WHEN b.sysadmin = 1 THEN 'sysadmin'
WHEN b.securityadmin=1 THEN 'securityadmin'
WHEN b.serveradmin=1 THEN 'serveradmin'
WHEN b.setupadmin=1 THEN 'setupadmin'
WHEN b.processadmin=1 THEN 'processadmin'
WHEN b.diskadmin=1 THEN 'diskadmin'
WHEN b.dbcreator=1 THEN 'dbcreator'
WHEN b.bulkadmin=1 THEN 'bulkadmin'
ELSE 'Public' END AS 'ServerRole'
FROM sys.server_principals a  JOIN master..syslogins b ON a.sid=b.sid WHERE a.type  <> 'R' AND a.name NOT LIKE '##%'

Script to find database users and roles assigned:

DECLARE @DBuser_sql VARCHAR(4000)
DECLARE @DBuser_table TABLE (DBName VARCHAR(200), UserName VARCHAR(250), LoginType VARCHAR(500), AssociatedRole VARCHAR(200))
SET @DBuser_sql='SELECT ''?'' AS DBName,a.name AS Name,a.type_desc AS LoginType,USER_NAME(b.role_principal_id) AS AssociatedRole FROM ?.sys.database_principals a
LEFT OUTER JOIN ?.sys.database_role_members b ON a.principal_id=b.member_principal_id
WHERE a.sid NOT IN (0x01,0x00) AND a.sid IS NOT NULL AND a.type NOT IN (''C'') AND a.is_fixed_role <> 1 AND a.name NOT LIKE ''##%'' AND ''?'' NOT IN (''master'',''msdb'',''model'',''tempdb'') ORDER BY Name'
INSERT @DBuser_table
EXEC sp_MSforeachdb @command1=@dbuser_sql
SELECT * FROM @DBuser_table ORDER BY DBName

Script to find Object level permission for user databases:

DECLARE @Obj_sql VARCHAR(2000)
DECLARE @Obj_table TABLE (DBName VARCHAR(200), UserName VARCHAR(250), ObjectName VARCHAR(500), Permission VARCHAR(200))
SET @Obj_sql='select ''?'' as DBName,U.name as username, O.name as object,  permission_name as permission from ?.sys.database_permissions
join ?.sys.sysusers U on grantee_principal_id = uid join ?.sys.sysobjects O on major_id = id WHERE ''?'' NOT IN (''master'',''msdb'',''model'',''tempdb'') order by U.name '
INSERT @Obj_table
EXEC sp_msforeachdb @command1=@Obj_sql
SELECT * FROM @Obj_table

Schneider Electric Việt Nam

Phần đính kèm
Database_Users_and_Roles.sql [785 Bytes]
Server_Level_Logins_and_Roles.sql [791 Bytes]
Object_Level_Permissions.sql [614 Bytes]
Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: