PME9.0 - PM8000 vista diagrams not fully translated into Chinese
Product Line
Power Monitoring Expert 9.0

Environment
Vista - Diagrams (Chinese language)

Issue/Cause
Some of the labels are not fully translated to Chinese for the PM8000 default diagrams in Vista.


Resolution
The workaround is to manually change the meter default diagrams (located at C:\Program Files (x86)\Schneider Electric\Power Monitoring Expert\config\diagrams\ud\default) to display the proper language.

Additional Information
This has been fixed in PME 2020.

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: