Unable to download to HMISTO7 over USB cable with Virtual Machine
Issue:
Download over USB cable fails to start when using a Virtual Machine (VMware, Fusion, etc) running EcoStruxure Operator Terminal Expert

Product Line:
HMISTO, HMIGTU, HMIST, EcoStruxure Operator Terminal Expert

Resolution:
When running EcoStruxure Operator Terminal Expert in a Virtual Machine (VMWare, Fusion, etc), ensure to set the USB Compatibility to version 1.1 if you require to download to the HMI via USB cable. If you leave it at 3.0 or 2.0, the USB download will not start.


Schneider Electric Việt Nam

Tìm hiểu thêm
Sản phẩm:
Bài viết có thể hữu ích
Tìm hiểu thêm
Sản phẩm: