What is electrical durability of relays in Altivar ATV320 variable speed drive?

Article available in these languages: Tiếng Thổ Nhĩ Kỳ

The two relays in Altiar 320 are different. For R1 relay, see pictures R1a, R1b. These are the data from relay manufacturers. Whether R1a or R1b is used in your product - it depends on relay availability from the supplier at the time Altivar was manufactured..
For R2 relay, there is only one supplier, see durability on picture R2. Example from curve, at 1A, electrical durability of R2 is 100x10000 cycles that means 1million cycles.
Pictures attached below are
R1a
R1b, R1b_1
R2

Schneider Electric Việt Nam

Phần đính kèm
R1a.jpg [114.36 KB]
R1b_1.jpg [92.01 KB]
R2.jpg [48.97 KB]
R1b.jpg [34.75 KB]
Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: