How to configure PowerChute Network Shutdown (PCNS) in Advanced UPS configuration with vSAN stretched cluster
Issue:
When PCNS is configured in Advanced UPS configuration with vSAN stretched cluster environment, then Witness VM is displayed in VM Prioritization page.

Product Line:
PowerChute Network Shutdown (PCNS)


Environment:
vSAN stretched cluster with Witness VM present in Datacenter.

Symptoms:
Witness Appliance (VM) is displayed in PCNS VM Prioritization page.
For VMware 7.0 (ESXi 7.0)

Resolution:
If PCNS is on a physical machine (outside cluster), then add the physical UPS Group to the last group, ie UPS Group 4, as shown in the example below.

Example: In a 2 node vSAN stretched cluster with Witness Appliance, configure PCNS with Advance UPS configuration and map Hosts to UPS Groups as below.
UPS Group 1 - vSAN host1
UPS Group 2 - vSAN host2
UPS Group 3 - Management host (VCSA) and Witness Appliance
UPS Group 4 – PCNS installed physical machine (unmapped group)

Recommendation: The recommended deployment for vSAN Stretched Cluster with Management Host (VCSA) is to place PCNS Appliance on the Management Host.

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: