HMIST6400 initial page does not appear if HMI target is not connected to PLC EOTE V3.1 SP1 There is one new feature called Drawing Mode added in V3.1 SP1. It is used to set the timing of changing the display when screen/content is changed (you can refer to SP1 online help). For this case, the workaround is to change the Drawing mode from screen priority to 3.1 compatible.
Đã phát hành cho:Schneider Electric Việt Nam