Configuration Manager Tool 2020 - "No matching constructor found on type" error when launching the tool
Issue
When first launching CM Tool 2020 on a server (usually older versions of OS) it will ask for .NET 4.6 to be installed as it is not present. After installing the .NET and rebooting the server the CM Tool will still fail to open and will throw the following error:
"No matching constructor found on type
'ConfigurationManager.ViewModels.ConfigurationManagerVM'. You can use the Arguments or FactoryMethod directives to construct this type.
"



Product Line
Configuration Manager Tool 2020

Environment
Upgrades
Migrations

Cause
This issue happens due to a missing .NET framework component.

Resolution
1) Apply all the outstanding Windows Updates on the server
2) Install .NET 4.7.2 framework

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: