Power Monitoring Expert v2020: Issue with Last row visibility and column width resize in Hierarchy Manager UI
Issue
In PME 2020 WebApp > Settings > System > Hierarchies screen Issue with Last row visibility and column width resize in Hierarchy Manager UI.
a>

b>
Environment
Power Monitoring Expert 2020 CU1/CU2


Cause
Issue is identified as bug in PME v2020.


Resolution
Apply PME 2020 CU2 (if not installed yet)
Refer KB article FA408541 for the same.

Download the attached file ‘jquery.event.drag-2.2.js’.
Copy the downloaded file in PME machine at the below location. (Note: before replacing, take original file backup)
"C:\Program Files (x86)\Schneider Electric\Power Monitoring Expert\Applications\SystemDataService\Content\Applications\HierarchyManager\Scripts\jQuery"

Close the Web application if it is open before copying the .js file.

Schneider Electric Việt Nam

Phần đính kèm
jquery.event.drag-2.2.js [12.53 KB]
Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: