What stand for the terms “Smartlink”, “Smartlink EL B” and “Smartlink ELEC”?

Smartlink is the generic name of the products to transfer data from Acti 9 devices to a superior system via the communication system.
Smartlink EL B is the product installed in electrical panel to connect with auxiliaries and perform the communication with the Cloud.
Smartlink ELEC consists in a Smartlink EL B product, a set of Ti24 auxiliaries, pulse energy meters, and analog sensors connected to Smartlink EL B, Cloud server service, as well as two Smartphone applications :
- Config ELEC for electrician for configuration and commissioning
- Smartlink ELEC for end user to remotely manage his electrical installation

Schneider Electric Việt Nam