What is the replacement external reset button for Class 8536 Type SAG, Type SBG, or Type SCG starter?
Issue:
What is the replacement external overload reset button on the 8536 Type S starters?

Product line:
NEMA starter, 8536 Type SAG SBG SCG (, sizes 00, 0, 1)

Environment:
NEMA and Definite Purpose Contactors and Starters

Cause:
Replacement parts

Resolution:
Part number for the external reset bar/button is 9066SC1.

Schneider Electric Việt Nam

Tìm hiểu thêm
Sản phẩm:
Phạm vi:
Tìm hiểu thêm
Sản phẩm:
Phạm vi: