Are the Altivar ATV28 drives repairable?
Issue:
Wondering if the Altivar ATV28 drives, are repairable?

Product Line:
ATV28

Environment:
All

Cause:
Repair

Resolution:
No, the Altivar 28 drives are not repairable. Since ATV28's are already obsolete, the recommendation is to replace the drive with a present drive.


Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: