What is the catalog number EZM72MC for the EZM metering?

Issue:
Product Design features

Product Line:
EZM metering equipment

Resolution:
This is a special mounting channel for installing EZM metering equipment. The channel measures 6 feet (72 inches) in length and can be cut to length as needed. Mounting holes must be drilled on site to accommodate local conditions. An EZM72MC channel can be used in place of the standard channels packed with each EZM enclosure.

NOTE: The standard channels are measured to match the width of each EZM enclosure.

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Tìm hiểu thêm
Phạm vi: