What is the amount of current imbalance required to trip the feature unit 9065 solid state overload relay?

Issue:
When will a Solid State Overload trip when there is current Imbalance

Product Line:
NEMA and Definite Purpose Contactors and Starter

Environment:
9065 Solid State Overload Relay

Resolution:
The unit is guaranteed to trip within 3 seconds at 25% phase current imbalance. It will start tripping at +/- 17% imbalance.

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Tìm hiểu thêm
Phạm vi: