EPS UPSs or SSC with GUI that the touch point is off
Public

Issue:
EPS UPSs or SSC with GUI that the touch point is off

Product line:
All EPS UPSs or SSC with GUI

Environment:
All EPS UPSs or SSC with GUI

Cause:
The touch point is off on the GUI and needs to be calibrated to reset touch point.

Resolution:
How to calibrate the GUI:
1.            Click on Start->Settings->Control Panel->Stylus->Calibration->Recalibrate.
2.            Calibrate the five point accurately.
3.            Press ENTER if keyboard is connected else TAP on the screen, it will exit the calibration screen.
4.            Save registry from Start->Programs->ColibriTools->SaveReg.

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: