Double click do not work Control Expert session is running on an extended monitors
If you have 3 additional displays configured as extended monitors, the double click function does not work on the extended monitor.  This occurs when Control Expert session is running on the extended monitor.

This issue has been fixed in Control Expert 15.   To resolve the issue, you need to upgrade to Control Expert 15 as a minimum.

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: