Can the BMXDDI3203 and BMXDDI3232 discrete input modules be used with Control Expert 15?
The BMXDDI3203 and BMXDDI3232 can be used with Control Expert 15.  The two input modules were released after CE15 was released and therefore requires a HotFix to be installed to allow their selection in the New Device IO Module pick list.

The HotFix file is 'ControlExpert_V150_HF_DDI_3232_DDI_3203.zip.' (see attachment)

The two extracted filenames are:
ControlExpert_V150_HF_DDI_3232_DDI_3203.exe
ControlExpert_V15_HF_DDI_3232_DDI_3203_ReadMe.mht


Follow the directions in the ReadMe to install the HotFix in Control Expert 15.

Schneider Electric Việt Nam

Phần đính kèm
ControlExpert_V150_HF_DDI_3232_DDI_3203.zip [11.54 MB]
Tìm hiểu thêm
Sản phẩm:
Tìm hiểu thêm
Sản phẩm: