Does the Panel Server Support ION Protocol ?
Product Line
EcoStruxure Panel Servers

Environment
Panel Servers + ION Meters (ION7650, ION9000, ION8xxx, PM8000)

Question
Does the Panel Server support ION protocol ?
Link150 has an ION Pass Through service. Is it the same for the Panel Server ?

Answer
ION protocol will not be supported by the Panel Server.
Only the Modbus Map of the ION meters will be supported.

Schneider Electric Việt Nam

Tìm hiểu thêm
Sản phẩm:
Bài viết có thể hữu ích
Tìm hiểu thêm
Sản phẩm: