Can I add additional terminals to Resi9 MP?
Issue:
I need an additional terminal with my Resi9 MP.

Product Line:
Resi9 MP

Resolution:
Yes, you can add additional terminals on already existing support or buy additional support and terminals if not provided in standard.

Notes:
The commercial reference for additional Terminal block support is MIP99036.
You can get more details on terminals blocks : MIP99037-38-39-40 .

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: