Cannot access the PowerChute Business Edition version 10.0.2 Agent web interface.
Issue:
Cannot access the PowerChute Business Edition version 10.0.2 Agent web interface. This may arise after upgrading from version 10.0.1 or a clean install. Also, you may see Windows Event ID 1067, and in the pcbe.log found in C:/Progarm Files (x86)/APC/PowerChute Business Edition/agent/log, you will see "Unable to load permanent storage m11.cfg.  If this file is corrupted, you may need to re-install".

Product:
PowerChute Business Edition version 10.0.2 Agent

Environment:
All supported Windows OS

Cause:
Security changes made to Agent 10.0.2

Solution:
Uninstall PowerChute Business Edition 10.0.2 and install PowerChute Serial Shutdown, available at
https://www.se.com/ww/en/product-range/137943580-powerchute-serial-shutdown

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: