How do I know if the wireless panel server is actually connected to the LoRa network?

Article available in these languages: Tiếng Hà Lan

You will know if the wireless panel server is connected to the LoRa network if it is already associated with EcoStruxure Facility Expert.
There are two different cases:
If the wireless panel server is already associated with Facility Expert:
  • The LED is solid green: the wireless panel server is connected.
  • The LED is flashing orange: the wireless panel server has lost the LoRa network.
The only way to ensure that the wireless panel server is connected without the association with Facility Expert is to use a LoRa tester. Note that you have the option to perform an eligibility test to estimate your coverage level.

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: