How to change the SiteManager Token Domain for Windows target?
For some reason, if you need to change the token domain of one SiteManager on Windows Target, you cannot just update the Domain Token name and reconnect. In this case, the SiteManager will still try to connect to the previous Domain Token
The goal of this FAQ is to explain how to do it

This article is applicable for the part SiteManager of EcoStruxure Secure Connect Advisor on Windows target

To update the Domain Token, need to reset the SiteManager information
To do it, need to execute the batch file ReConfig SiteManager Embedded located in SiteManager folder
Capture.PNG

After executing the batch file, all information of SiteManager will be reset and you will be able to change the Domain token

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: