Can TeSys Giga contact wear diagnostic feature indicate if the contact tips melt ?

Article available in these languages: Tiếng Hà Lan

Contact wear diagnostic feature has an inbuilt algorithm which continuously estimate, the main contacts opening speed. During each opening it determinate the wear level based on the Initial state and the speed estimation. And this shall help to precisely indicate the end of life by the self-diagnosis LED.
This function will not detect contact welded.

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: