Where is the access level in the ATV320 drive?

Article available in these languages: Tiếng Nhật

Issue:
Not able to find the access level (LAC) parameter in ATV320 drive

Product Line:
ATV320

Environment:
ATV320 all series

Cause:
Trying to find the  LAC parameter in ATV320 drive, but not able to find it.

Resolution:
On the keypad:
Go to ConF, Full and then look for LAC (access level)
Options are:   Basic (bAS); Standard (Std); Advanced (Adv); Expert (EPr).
Expert will allow you to work without restrictions in the drive.

In SoMove:
Go to “Parameters” tab, then go to “Full” in the left side menus and it will show the Access level parameter in the right area.

Schneider Electric Việt Nam

Tìm hiểu thêm
Sản phẩm:
Tìm hiểu thêm
Sản phẩm: