What is the In-rush current of the HMISTW6/HMIST6?
On Schneider Electric website (www.se.com), the inrush current of different HMIs is provided with the unit A (Ampere): For example, the inrush current of the HMISTW6400 is 30 A. This comparatively high inrush current makes our customers wonder.
The goal of this article is to provide the inrush current with the unit: A²*s like our competitors.

This article is applicable to the following products:
HMISTW6, HMIST6

Find below the inrush current of the HMISTW6/HMIST6 with unit A²*s:
SeriesDisplay sizeIn-rush current
Harmony ST6
Harmony STW6
4w”/7” w0.2 A²*s
10” w/12” w/ 15” w0.6 A²*s

Schneider Electric Việt Nam

Tìm hiểu thêm
Sản phẩm:
Bài viết có thể hữu ích
Tìm hiểu thêm
Sản phẩm: