What is an SOF fault on the ATV12?

Article available in these languages: Tiếng Tây Ban Nha

Issue:
SOF fault on ATV320

Product Line:
Altivar Machine, ATV12

Environment:
All serial numbers

Cause:
• Instability
• Overspeed associated with the inertia of the application

Resolution:
• Check the motor
• Overspeed is 10% more than Maximum frequency tFr page 57 so adjust this parameter if necessary
• Add a braking resistor
• Check the size of the motor/drive/load
• Check parameters of the speed loop (gain and stability)

ATV user manual:
https://www.se.com/ww/en/download/document/BBV28581/

Schneider Electric Việt Nam

Phần đính kèm
ATV12_user_manual_EN_BBV28581_04.pdf [3.62 MB]
Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: