What causes an input phase loss PHF fault on the ATV12?
Issue:
Getting a input phase loss PHF fault on ATV12

Product Line:
Altivar Machine, ATV12

Environment:
All serial numbers


Cause:
• Drive incorrectly supplied or a fuse blown
• Failure of one phase
• 3-phase ATV12 used on a 1-phase line supply
• Unbalanced load
• This protection only operates with the drive on load

Resolution:

• Check the power connection and the fuses.
• Use a 3-phase line supply.
• Disable the fault by setting Input Phase loss detection IPL page 94 = nO.
• Check the motor connection and any isolating devices located between the drive and the motor (contactors, circuit breakers, etc.).


ATV12 user manual:
https://www.se.com/ww/en/download/document/BBV28581/

Schneider Electric Việt Nam

Phần đính kèm
ATV12_user_manual_EN_BBV28581_04.pdf [3.62 MB]
Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: