Issue
Planning on using the BMENOC0301 or BMENOC0311 in a configuration where RSTP is not allowed and need to disable this feature.
Product line
Modicon M580, Control Expert
Resolution
As of June 14, 2023 (v2.21) there is no way to disable RSTP. If you need a port without RSTP you can use the service port. The service port of the BMENOC03x1 modules does not support RSTP.
Đã phát hành cho:Schneider Electric Việt Nam