What is the appropriate level of RSSI signal on a NetBotz wireless sensor?
Issue:
What is the appropriate level of RSSI signal on a NetBotz wireless sensor?

Product Line:
NetBotz

Environment:
NBRK0250
NBRK0450
NBWL0455
NBRK0550
NBRK0570
NBRK0750
NBWL0755
NBWS100H
NBWS100H
NBWS100T
NBPD0180
NBWC100U

Cause:
Low RSSI can lead to communications issues and dropped sensors.

Resolution:
It is recommended that the wireless sensors and routers be kept at 80% RSSI and above.

If you set the wireless network up, especially during off hours, there may be spikes in wireless usage from other devices or other interference from other network components once the environment is fully in use that can cause lower RSSI values and in turn, communications issues.

If you configure the wireless network and have a lower RSSI and the sensors appear to be intermittent, the first recommendation is to try to reconfigure to get a better RSSI

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: