What does triangle with exclamation mark on the Display for the iEM3000 represent?
Answer
Issue
What does triangle with exclamation mark on the Display for the iEM3000 represent?
_____________________________________________________________
Product Line
iEM3000 series meters
_____________________________________________________________
Environment
Power Monitoring Expert (PME)
ION Setup
Modbus mastering
_____________________________________________________________
Solution

The triangle icon will be displayed in iEM3255 if any acknowledged alarm is active.

Once the alarm is acknowledged, this will disappear.


Iem3255-Triangle icon-Final.jpg

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: