undefined undefined
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
Can a BMXCPS4002S and BMXCPS4022S redundant power supplies be used together in a redundant rack?
Different redundant power supply models are allowed in the same redundant rack as shown below.  They do not have to be of the same model number.

In this example, a BMXCPS4022S (24-48 VDC input) and a BMXCPS4002S (100-240 VAC input) are installed.
It is normal to have two different voltage sources powering a rack.
BMXCPS4022S and BMXCPS4002S redundant power supplies


Schneider Electric Việt Nam

Tìm hiểu thêm
Sản phẩm:
Tìm hiểu thêm
Sản phẩm: