How can you set up the ATV630 and ATV930 drive for sourcing or sinking logic inputs?

Issue:

ATV630 and ATV930 drive for sourcing or sinking mode?

Product Line:

ATV630 and ATV930 Family

Environment:

All

Cause:

Setting up the logic inputs to switch on with a sinking input to com.

Resolution:

The sink source switch is located on the face of the drive under the terminal IO block. Sink position is on the left and source position is on the right.

sink or source image I

Sink or Source image II

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: