Why doesn't eSetup detect the EVlink Pro AC ?
Check that the EVlink Pro AC is powered ON with the strip light green.
Check that you are close to the EVlink Pro AC, less than 15 meters away.
Check that Bluetooth is activated on your smartphone or tablet.
Check that you have not entered 3 faulty pin codes.
Check that you have the right name of the charging station.
If the above is OK, it means the Bluetooth is not active on the EVlink Pro AC, in which case you can:
1- Activate the Bluetooth by powering the charging station Off and then On, and wait for the strip light to turn green.
2- Tap the admin badge on the RFID reader. The Bluetooth of the EVlink Pro AC will be activated for 2 hours.

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: