Why, in EcoStruxure Machine SCADA Expert, sometime the Site Code cannot be generated?
In EcoStruxure Machine SCADA expert, there are two kind of license
  • Hardkey
  • Softkey
When softkey is using, the license is linked to the Site code of one of your network card.
To find the Site Code, need to start "EcoStruxure Machine SCADA Expert 2020 Register" and select SoftKey

In some specific cases, the following error may occur
error message

This FAQ will show how to avoid this error message

This article is application for EcoStruxure Machine SCADA Expert, all versions

This error may occur, when there are too much network card in the configuration.
The solution to be able to create the SiteCode in this situation, is to desactivate the not necessary network card and let only the main one.
workaround
In general this action is enough to fix the problem and generate the Site Code.
If the problem still occur, do not hesitate to contact the technical support

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: