What is the part number of the Memory Key for the Safety Logic Controller TM5CSLC100FS and TM5CSLC200FS?
Issue:
Part number for the TM5 Safety Logic controller


Product Line:
TM5, SoSafe


Resolution:
A memory key is required for operation of the Safety Logic Controller, and is sold separately.
The table below presents the part number for the memory key
Part number Description color
TM5ACSLCM8FSSafety Logic Controller memory key, 8 MbGray and red

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: