Tìm các câu hỏi thường gặp
What is the password used for the Zelio relay inside the enclosed ATV660 Drives?
Issue:
ATV660 enclosed Zelio relay password
Product Line:
ATV660, ATV960
Environment:
All
Cause:
Needs to access the password to look at the program or to change the program.
Resolution:
The default password for the Zelio relay is 6601 however according to the manufacturing plant some may have been shipped out with password 6101 and 6201.
Đã phát hành cho:Schneider Electric Việt Nam
Tìm hiểu thêm
Phạm vi:
Tìm hiểu thêm
Phạm vi: