Can I update the M580 CPU’s firmware via the BMENOC03xx module?
Issue:
Firmware update the M580 CPU’s firmware via the BMENOC03xx module


Product Line:
M580


Resolution:
Yes, you can connect the BMENOC03xx module’s embedded Ethernet switch to the CPU. Check that the BMENOC03xx module is running properly before starting the update procedure.
You cannot, however, update the CPU if Unity Loader is connected on the BMENOC03xx module’s IP address.

Schneider Electric Việt Nam

Tìm hiểu thêm
Sản phẩm:
Bài viết có thể hữu ích
Tìm hiểu thêm
Sản phẩm: