Yes. The Evlink Pro AC measures the reactive current. If the reactive current is higher than 2,5A phase by phase during 1 minute, the floor value will be 14A for 3-phase charging or 8A for single-phase charging.
Đã phát hành cho:Schneider Electric Việt Nam