What is the purpose of the Transfer Tool that is installed with EcoStruxure Machine Expert Basic?
Issue:
Purpose of the Transfer Tool that is installed with EcoStruxure Machine Expert Basic


Product Line:
EcoStruxure Machine Expert Basic


Resolution:
The Transfer Tool is a console application allowing scripting operations without using EcoStruxure Machine Expert - Basic.
The Transfer Tool allows you to:
  • Download and upload the project to and from the controller.
  • Update the controller firmware.
  • Backup and restore application data.
NOTE: To use the Transfer Tool, you must connect the PC to the controller using a USB cable.

Schneider Electric Việt Nam

Tìm hiểu thêm
Sản phẩm:
Bài viết có thể hữu ích
Tìm hiểu thêm
Sản phẩm: