What diode is used for inductive output protection BMXDAO1605 as specified in the specifications?
The Modicon X80 Discrete Input/Output Modules User Manual, 35012474.18, page 259, states there is no protection against inductive over voltage and recommended a discharge diode on each output.  See highlighted below.

Since the reference to diodes would apply to DC applications, the reference will be removed from the User Manual.

BMXDAO1605 specification


Schneider Electric Việt Nam

Tìm hiểu thêm
Sản phẩm:
Bài viết có thể hữu ích
Tìm hiểu thêm
Sản phẩm: