How can I setup an XBTF Magelis HMI to communicate to a M580 via Modbus RS232?
Issue:
XBTF communication to a M580 serial port via RS232


Product Line:
XBTF, M580


Resolution:
For RS232 communication between the Magelis XBTF and M580 PLC, you must use the BMXNOM0200 serial communication module. The communication cable between the XBTF HMI and NOM module is shown below.

image1

The NOM module Channel 0 must be configured for Modbus RS232 as shown below
image2


The XBTF configuration( Baud rate, Parity, stop bit and Timeout between frames) should match the serial port setup of the BMXNOM0200 module.
image3

Schneider Electric Việt Nam

Tìm hiểu thêm
Sản phẩm:
Bài viết có thể hữu ích
Tìm hiểu thêm
Sản phẩm: