Issue:
Where can we find the download links for Vijeo Designer V6.2 SP12?
Product Line:
Vijeo Designer V6.2 (all hotfixes and service pack revisions less than SP12)
Resolution:
Please find the download links for Vijeo Designer V6.2 SP12 below. Please download the zip file and extract it to get the exe.
You must have Vijeo Designer 6.2 already installed.
Each SP is cumulative so you do not need to install SP1-10 first.
*NOTE: In order to successfully install the service pack or any of the related packages, always right-click on the exe file and select "Run as Administrator". This will ensure the installation is completed properly.
The Vijeo Designer Data Manger is for a standalone install ONLY. There is no need to install the tool with the full install of the Vijeo Designer development environment. It comes pre-installed already.
Đã phát hành cho: Schneider Electric Việt Nam