NetBotz IP information disappears after hostname or DHCP change
Issue:
NetBotz IP information disappears after hostname or DHCP change

Product Line:
NetBotz 5.x

Environment:
NBRK0750
NBWL0755

Cause:
When the hostname is changed on a NetBotz 750/75 or the settings are changed from manual to DHCP, the IP information disappears from the System --> Network configuration page.

Resolution:
The information is not lost, it is still in the NetBotz appliance. By simply clicking to another page and back, or refreshing the network page, the information should again be visible on the Network page.

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: