Is Profinet communication Protocol available for any of the Schneider Electric VFDs?
Issue:
Availability of Profinet communication option on Altivar drives?

Product Line:
ATV630, ATV930, ATV320, ATV340, APM, ATV32

Environment:
All

Cause:
NA

Resolution:
The part number for Profinet option card is VW3A3627. It is compatible with:
Altivar Process ATV600
Altivar Process ATV900
Altivar Machine ATV340 except Sercos drives
Altivar Machine ATV320
Altivar 32
Altivar Process Modular(APM)

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: